Use duplicate destructive bit detection

Use duplicate destructive bit detection to find duplicate destructive bit references.
  1. In the
    Execution Pane
    , select the controller.
  2. Right-click and select
    Find duplicate destructive bits
    . The
    Duplicate destructive bit references
    window opens with the list of all the duplicated destructive bit references in the controller. If no duplicate destructive bits are found in the controller, no references will show in the window and you will see a message that says no duplicate destructive bits were found in the controller. The window lists the tag bits and the locations of destructively duplicated references for these tags and parameters of these scopes:
    • Controller
    • Program
    • Routine
    • Smart Object program
    • Smart Object routine
    • AOI parameter
  3. Hover over a row to highlight it.
  4. Double-click the row to navigate to the instruction to fix the destructively duplicate reference.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.