Array (File)/Shift Instructions
Use the array (file)/shift instructions to modify the location of data within arrays.
Available Instructions
Ladder Diagram
You can mix data types, but loss of accuracy and rounding error might occur.
The bold data types indicate optimal data types. An instruction executes faster and requires less memory if all the operands of the instruction use the same optimal data type, typically DINT or REAL.
Provide Feedback