Reset an APR Fault
There are three ways to reset an APR Fault.
- Instruction ExecutionExecuting an MAFRExecuting an MGSRExecuting an MASRExecuting an MCSR
- From the Controller Organizer:Clear the group fault, theLogix Designerapplication executes an MGSRClear the axis fault, the application executes an MASR
- Downloading the same project a second time
Provide Feedback