DINT to SINT or INT

To convert a DINT value to a SINT or INT value, the controller truncates the upper portion of the DINT and sets the overflow status flag, if necessary. The following example shows the result of a DINT to SINT or INT conversion.
For example, the conversion of a DINT to an INT and a SINT:
This DINT value:
Converts to this smaller value:
16#0001_0081 (65,665)
INT
16#0081 (129)
SINT
16#81 (-127)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.