Sequencer Instructions

Sequencer instructions monitor consistent and repeatable operations.
Available Instructions
Ladder Diagram
If you want to
Use this instruction
Detect when a step is complete.
Set output conditions for the next step.
Load reference conditions into sequencer arrays
The
bold
data types indicate optimal data types. An instruction executes faster and requires less memory if all the operands of the instruction use the same optimal data type, typically DINT or REAL.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.