Understand Instruction Timing

Motion instructions use three types of timing sequences:
Description
Timing Type
The instruction completes in one scan.
The instruction completes over several scans because the instruction sends messages to the servo module.
The instruction could take an indefinite amount of time to complete.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.