Minor Recoverable Fault
If a minor fault occurs for: | This field displays: | That may indicate: |
Digital module | Multicast CRC errors above threshold | The module is confused about which slot it is in because too many multicast CRC errors have occurred |
RA/GA miscompare fault | ||
Multicast receiver disabled | ||
Analog input module | Channel Fault | Calibrating, underrange, or overrange on at least one channel |
Analog output module | Channel Fault |
|
Non I/O module
I/O (input/output) Devices that provide and/or receive data from the controller. | Faulted |
|
If the software configuration and the actual physical hardware differ greatly (such as, the software has been configured for a digital module and the actual physical module is an analog module), then the software can only display this generic fault status:
fault
A problem or error detected by the control system hardware or software. A fault is identified by an error code or an error bit.
- Unrecoverable Fault
- Recoverable Fault
- None
Provide Feedback