Gain Results Tab - FLEX I/O Analog

This tab shows you the results of the input channel gain calibration. You can see the results in the
gain
The ratio of the magnitude of the output signal with respect to that of the input signal.
In a linear equation (y=mx+b), the parameter (m) is used to drive the dependent variable (y) to a specified value when the independent variable (x) is at a maximum.
Status
column.
If the Status column displays:
Then:
OK
Click
Next
to perform gain calibration on the output channels.
Error
Click
Retry
to repeat the process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.