Gain Tab - FLEX I/O Analog
This tab allows you time to attach a meter to a channel of the FLEX I/O analog module.
Use the following buttons to perform your desired action:
Retry
Select this button if an error occurs and you need to repeat a step in the calibration process.
TIP:
This button is only enabled when an error occurs.
Next
Select this button to produce the high reference signal.
Stop
Select this button to cancel calibration and exit the calibration.
Help
Select this button for assistance with this tab.
Provide Feedback