Low Clamp Limit greater than High Clamp Limit
The Low Clamp Limit is greater than or equal to the High Clamp Limit. Enter a Low Clamp Limit that is less than the High Clamp Limit.
- The High Clamp Limit is the highest value an output module will be allowed to reach in the control process.
- The Low Clamp Limit is the lowest value an output module will be allowed to reach in the control process.
Provide Feedback