Module Properties Dialog Box - Setup Tab Overview (1756-DM, PowerFlex 700S and PowerFlex 700SE with DriveLogix5720, PowerFlex 700S 2 and PowerFlex 700Se2 with DriveLogix5730, PowerFlex/DPI, SCANPort)
Use this tab to:
- launch DriveTools 2000
- associate a DriveTools 2000 file with a module
- update module configuration data with DriveTools 2000 link information
Parameters
Drive File
Displays the name of the DriveTools 2000 file that is to be associated with the selected module. By default, this field is blank.
Browse
Click this button to search for the file you wish to associate with the selected module.
Project Directory
Displays the location where the new file will be stored if you don't provide directory information for the Drive File.
(View Parameter Data In Drive File Button)
Click this button to view and edit parameter and link data associated with this drive. Data is stored in the Drive File.
Status
Displays the status the controller has about the module:
This status: | Indicates: |
Standby | a transient state that occurs when shutting down |
Faulted | the controller is unable to communicate with the module When the status is Faulted, the Connection tab displays the fault. |
Validating | a transient state that occurs before connecting to the module |
Connecting | a state that occurs while the connection(s) are being established to the module |
Running | the module is communicating and everything is working as expected |
Shutting Down | the connections are closing |
Inhibited | the connection to the module is inhibited |
Waiting | a connection to this module has not yet been made due to one of the following:
|
Offline | you are not online |
OK
Click this button to accept your edits and close the dialog box.
Cancel
Click this button to cancel your edits and close the dialog box.
Apply
Click this button to apply your edits and continue editing box.
Help
Click this button for help on this tab.
Provide Feedback