Output Calibration Dialog Box - Gain Results Tab Overview (FLEX I/O Analog)

The purpose of this tab is to:
  • show you the results of the gain calibration
    gain
    The ratio of the magnitude of the output signal with respect to that of the input signal.
    In a linear equation (y=mx+b), the parameter (m) is used to drive the dependent variable (y) to a specified value when the independent variable (x) is at a maximum.
  • notify you that calibration is complete
  • give you the ability to return to the Calibration tab
You can see the results in the Status column.
If the Status column displays:
Then:
OK
Calibration is successfully complete.
Error
Click Retry to retry to show the results of the gain calibration and notify you that calibration is complete.
TIP:
You must click the Finish button to return to the Calibration tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.