Pulse Width Modulation PWM
The 1794-VHSC module can generate a pulse width modulation signal that may be tied to any output. By specifying a Time Base period and Gate Interval when Pulse Width Modulation is selected for the type of input counter, a counter and its first ON/OFF window comparator are assigned and the signal is generated.
Provide Feedback