Rate Alarm negative
The current Rate Alarm setting is negative and negative Rate Alarms are not allowed. Enter a non-negative Rate Alarm setting.
The Rate Alarm value indicates to trigger when the rate of change between input samples exceeds the setpoint. You must set this alarm in terms of Engineering Units/Second.
Provide Feedback