View Output Gain Results (FLEX I/O Calibration)
To view the results of the gain calibration:
gain
The ratio of the magnitude of the output signal with respect to that of the input signal.
In a linear equation (y=mx+b), the parameter (m) is used to drive the dependent variable (y) to a specified value when the independent variable (x) is at a maximum.
- Look at theStatuscolumn.IF:
- OKappears, calibration is successfully complete.
- Error appears, selectRetryto retry to view the results of the gain calibration and notify you that calibration is complete.
- SelectFinish.The software returns you to theCalibrationtab.
You may also select
Help
for assistance with this tab.Provide Feedback