GroupOverlapFault
Applies to: Axis Groups.
GroupOverlapFault is a Boolean attribute. It is set when the
Logix Designer
application processor has been unable to execute the current motion task before another motion task is scheduled in the motion task queue. This fault is usually the result of setting a Coarse Update Period in the Attributes tab of the Motion Group properties dialog box that is too low.GroupOverlapFault is a recoverable fault.
To clear a GroupOverlapFault:
- Diagnose and fix the underlying problem (for example, increase the Coarse Update Period).
- Be sure your program or fault handling routine contains a Shutdown Reset (MGSR) instruction to return to the axis ready operating state.
A GroupOverlapFault sets the GroupFault attribute.
Provide Feedback