<Component type> <component name> is not defined in import file or in project Message
There are undefined references that do not collide with anything in the project.
The
Operation
field is set according to configuration operations rules.Provide Feedback