Import/export Logic Comments command
Import logic comments from an ASCII CSV file and export logic comments to an ASCII CSV file.
To import logic comments command
- From theToolsmenu, chooseImport.The Import dialog box opens.
- Enter the name and location of the CSV file to import comments.You do not need to add a file extension. If you do, use the CSV extension.
- Choose aLogic Comment Collisionoption.
- SelectImportto import the logic comments.
Special characters in the CSV file may fail to import. The Import command may fail if special characters (for example, =, +, ", ', -) are included in the tag description and the CSV file was edited using Microsoft Excel software. The CSV import process requires and verifies that all descriptions adhere to the IEC-61131 naming standard. In the imported file, the sequence "= is not allowed.
IEC-61131 Name Standard
(The names are composed per IEC-61131, section 2.1.2.)
An identifier is a string of letters, digits, and underline characters that begin with a letter or underline character. Underlines are significant in identifiers (for example, A_BCD is interpreted differently than AB_CD). Multiple leading or multiple (consecutive) embedded underlines are not allowed, trailing underlines are not allowed, and letter case is not considered significant.
TIP:
In Logix Designer, most component names are limited in length to 40 characters or less.
Note that when importing or exporting to a CSV file, Microsoft Excel software can only display Arabic characters. If you are using an Asian character set, use the .txt format to import or export.
To export logic comments command
TIP:
Only export logic comments if you have a profile file open.
- From theToolsmenu, chooseExport.The Export Tags dialog box dialog box opens.Export
- InFile name, enter a name for the export file.You do not need to add a file extension. If you do, use the CSV extension.
- SelectExportto export the project file.If you are offline, and there are one or more properties dialog boxes withPending edit pending edits, the edits are automatically applied.offlineA state in which a device is not in direct communication (for example, when programming inLogix Designer).
Provide Feedback