Program or Data Will Be Overwritten Messages

Existing [Standard | Safety] program will be overwritten with a [Safety | Standard] program
A safety or a standard program collides with an unscheduled existing program that has a different class type and the imported program is being imported either as unscheduled or into a task with the same class type as the imported program and the Operation field is set to Overwrite.
The Operation field is set according to configuration operations rules.
If the delete of <deleted tag name> is the result of a rename, online data values will be overwritten.
A program or phase-scoped tag is being deleted online and there is at least one program or phase-scoped tag being created with the same data type and Alias For attributes.
The online data values of the renamed tag are overwritten with the initial values of the new tag.
The Operation field is set to Delete.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.