Unable to Create Messages

Unable to create <component type> <component name>
Access limitations prevent this import component or referenced component from being created.
The final name replaces the import name for all references in the imported logic (if a reference component and the Final Name are different from the import name.)
The Operation field is set to Discard.
Unable to create <component type> <component name>
A referenced tag is a motion type tag or safety component or produce/consumed tag or any other component that cannot be created or modified online.
The final name replaces the import name for all references in the imported logic.
The Operation field is set to Discard.
Unable to create all components of <component type> <component name>
An imported component (program, equipment phase, or Add-On Instruction) is prevented from being created or modified (that is, the software has forced the operation of one or more components to Use Existing or Discard).
The Operation field is set to Use Existing.
Unable to create or modify all components of <component type> <component name>
An imported component (program, equipment phase, or Add-On Instruction) is prevented from being created or modified (that is, the software has forced the operation of one or more components to Use Existing or Discard).
The Operation field is set to Use Existing.
Unable to create tag <tag name>
A referenced tag is program-scoped and existing program logic is referring to a controller-scoped tag by the same name.
Tag cannot be imported online. Imported logic references existing controller-scoped tag final name replaces the import name for all the references in the imported logic) unless the final name is changed).
The Operation field is set to Discard.
Unable to create tag <final name>
The final name for a tag reference is an invalid name.
The final name replaces the import name in all references in the imported logic.
The Operation field is set to Discard.
Unable to create [program | equipment phase] <program/phase name> in task
If you are offline or online in Program mode, the imported program or imported equipment phase is scheduled in a task or folder that has the maximum items allowed in it and it does not collide with an existing component in that folder or it collides with an existing program or phase in a different task or folder.
To create a new program or equipment phase, change the schedule in location.
The Operation field is set to Discard.
Unable to create program <program name>
The program is being imported into a Task in a Safety Controller and the Program and Task Class attributes are not the same (for collision cases, the existing program is unscheduled).
To create a new program, change the schedule in location.
The Operation field is set to Discard.
Unable to create program <program name>
The imported safety program cannot be scheduled in Controller Fault Handler or Power-Up Handler.
To create a new program, change the schedule in location.
The Operation field is set to Discard.
Unable to create motion group <motion group name>
A motion group tag is being imported with a different name than the existing motion group in the project.
The Operation field is set to Discard.
Unable to create equipment phase <equipment phase name>
The equipment phase component is the same name as an existing controller-scoped tag that is not of PHASE type.
To create a new equipment phase, change the final name.
The Operation field is set to Discard.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.