Plug-in applications
Plug-ins are add-on software components that provide functionality in addition to the functionality in the
Logix Designer
application. They can provide unique capabilities for working with your projects in the Logix Designer
application.You can use plug-in applications to add custom properties to projects. The custom properties are stored with the project file and are accessible when you open the project in the
Logix Designer
application. They are downloaded to the controller and are imported and exported with the project.Provide Feedback