Program Properties Dialog Box - Configuration Tab Overview
Define program execution properties from the
Configuration
tab of the Program Properties
dialog box.
TIP:
To open the Program Properties dialog box:
- From either the Controller Organizer or Logical Organizer, right-click the program to change and chooseProperties.
Parameter | Description |
Assign Main Routine | Select the Main routine assigned to this program from the pull-down menu. |
Assign Fault Routine | Select the Fault routine assigned to this program from the pull-down menu. |
Inhibit Program | Select the Inhibit Program check box if you want to prevent the controller from executing this program. The check box is cleared by default.This check box is not shown if the Use as Folder check box is selected on the General tab. |
Synchronize Redundancy Data after Execution | Select the Synchronize Redundancy Data after Execution check box to synchronize data at the end of the program execution.
TIP:
The
Synchronize Redundancy Data after Execution option only applies to standard controllers; it does not apply to Safety controllers.This check box is not shown for non-Redundancy catalog numbers or if the Use as Folder check box is selected on the General tab. The check box is always enabled for controllers with Redundancy enabled as long as the controller is not in Hard Run mode. The check box appears dimmed when Redundancy is not enabled. |
OK | Click this button to apply your edits and close the Program Properties dialog box. |
Cancel | Click this button to cancel your edits and close the Program Properties dialog box. |
Apply | Click this button to apply your edits and continue editing in the Program Properties dialog box. |
Provide Feedback