Delete a program
A program contains routines, including a main routine, and tags and is scheduled in a task.
Delete programs either from the
Controller Organizer
or the Logical Organizer
. Deleting a parent program also deletes its descendant programs. The
Delete
command is disabled if:- Security does not allow deleting the program.
- The immediate parent of the program is a program or a folder that security does not allow deleting
If the project is offline, delete a program from the organizer without having to unschedule the program and delete its routines and tags.
To delete a program:
- If the project is online, unschedule the program to delete from the task in which it is scheduled.
- Select the program in the Controller Organizer or Logical Organizer.
- From theEditmenu, chooseDelete.
- ClickYesto confirm the deletion.
Provide Feedback