Loading
Case Study
Recent ActivityRecent Activity
6 minute read

Mitsubishi Chemical Performance Polymers Uses Modular Control System, Manufacturing Intelligence to Launch New Plant in Brazil

Modular design speeds up plant deployment while remote access to information reduces startup challenges

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Mitsubishi Chemical Performance Polymers Customer facility

Challenge

  • Establish a new production facility in Brazil on an accelerated timeline and give on-site workers and external experts visibility into quality and production issues

Solutions

  • Modular Design Approach - System was designed, built and tested in the U.S. by Apex Control Specialists, then shipped and quickly installed in Brazil
  • FactoryTalk - FactoryTalk Historian, FactoryTalk View and FactoryTalk VantagePoint EMI software combined with CompactLogix PLC and PowerFlex 755 AC drives provide access to manufacturing intelligence
  • EtherNet/IP supports real-time communications and remote monitoring

Results

  • Modular system reduced facility deployment time by three to four months
  • Remote experts helped resolve early production issues
  • EtherNet/IP reduced I/O count by 70 percent
  • Information software gives operators key insights into quality

Consumers in places like the U.S., Japan and most of Europe take it as a given that their new vehicles will come equipped with an airbag. The safety feature became prevalent in vehicles in many developed countries during the 1990s. And by the turn of the century, it was either required by law or considered an essential component for automakers to include in their vehicles to achieve desired safety ratings.

But the same can’t be said in many developing and emerging countries around the world, where airbags still either aren’t required or aren’t commonly found. This was the case for car owners in Brazil until just recently. In 2014, a new law took effect requiring that airbags and other safety technologies be installed on all new vehicles sold in Brazil.

Brazil’s new airbag requirement was the driving force that led Mitsubishi Chemical Performance Polymers (MCPP)

to establish a greenfield production facility in Brazil, the world’s seventh-largest car market
. The new facility would primarily support the automotive market, supplying resins to airbag manufacturers for use in safety-critical airbag covers.

Prior to expanding to Brazil, MCPP already had been a leading global supplier of custom automotive materials for more than 30 years. The company had operations in 16 countries around the world, and provided solutions for fuel management, interior, exterior, wiring and other automotive applications.

However, building a facility from the ground up on a new continent – while also meeting key quality, safety and production demands – would be no easy task.

The Need for Speed

With an industrial site north of Sao Paulo selected as the location for its new production facility in Brazil, MCPP wanted to get production up and running as soon as possible to help local auto suppliers meet the impending airbag requirement.

“We wanted the start of production to coincide as closely as possible with the timing of the new airbag requirement,” said Lee Wilson, plant manager for MCPP. “The harsh rain season pushed our site work behind schedule somewhat. When that happened, it became all the more important to look for ways to be efficient in launching this new location.”

In terms of the production infrastructure, the new facility required a feeder and extrusion system that could produce up to about 10 million pounds of resin per year at maximum production capacity. Wilson and his team wanted the Brazilian plant to mimic what MCPP already had in other regions in terms of production speed and especially quality management.

“Quality was our first priority,” Wilson said. “We needed to make sure we could maintain tolerances with the feed systems that were feeding the extruder, as well as achieve proper distribution and dispersion of the various ingredients inside the extruder. Aesthetically, we needed to be able to maintain a consistent product look as material is compounded and pelletized.”

Visibility into the system would be essential to helping operators monitor quality and quickly take action on any production issues that may arise. Additionally, there was a desire to provide remote access into the system. This would allow U.S.-based MCPP employees and other outside experts to troubleshoot or diagnose technical challenges, and help compensate for a lack of local technical support in Brazil.

A Modular Approach

MCPP evaluated two vendors and ultimately chose Indiana-based Apex Engineering and its subsidiary Apex Controls Specialists, a Rockwell Automation Recognized System Integrator, to develop the extrusion system for its new Brazilian production facility.

Apex Engineering proposed a solution based on its Apex Modular Extrusion™ system. The system has a material-handling system at its top level that receives raw materials, including various rubbers, oils, heat stabilizers, impact modifiers and pigments. Those materials are distributed via a feeder deck down to the extrusion system, where they are heated and blended, and finally sent to an underwater pelletizing system that produces the final bead-like product. That product is then packaged into large bags and boxes, which are shipped to the airbag manufacturers.

A compounding control center houses the extrusion system’s electrical and control infrastructure, including an Allen‑Bradley® CompactLogix™ programmable logic controller (PLC), Allen‑Bradley PowerFlex® 755 AC drives, and solid-state relays from Rockwell Automation. A separate utility control center houses the system’s utilities and information server.

The information-enabled system gives workers and outside experts visibility into critical manufacturing intelligence, including temperatures, feed-rate pressures and feeder motor speeds. FactoryTalk® Historian software from Rockwell Automation collects thousands of these data points throughout the production process, while FactoryTalk View HMI software and FactoryTalk VantagePoint® enterprise manufacturing intelligence (EMI) software allow workers to manage recipes, monitor processes, and identify and resolve production issues.

Communications over EtherNet/IP™ allow the manufacturing intelligence to be shared plant-wide and with outside experts via remote access, while also reducing wiring in the MCPP facility.

Rapid Deployment

The extrusion system’s modular design proved crucial in helping MCPP speed up the launch of its new facility.

While construction of the plant was underway in Brazil, Apex was simultaneously designing and building the system in Evansville, Indiana. Wilson and his team at MCPP kept in close touch with Apex engineers during this process through weekly calls. Once the extrusion system was complete and operational, they were on-site with Apex personnel for a week of testing.

“We crawled all over the equipment,” Wilson said. “It was great being able to see the equipment running and test it firsthand. We only made small changes, but it was nice being able to make them before shipping the equipment to Brazil. It helped us avoid production delays and saved us some long flights to Brazil.”

Once the equipment arrived in Brazil, an on-site contractor quickly and easily assembled the system in a paint-by-numbers approach. The system’s power and electricals, for example, were all set up on connectors. Workers only needed to pull cables from cable trays and plug them in. Similarly, the system’s mechanicals had an accompanying drawing with easy-to-follow instructions for bolting the system together.

In total, the system took only about one month to install at the Brazilian facility. This saved MCPP as much as four months in deployment time. It also allowed the company to finish the extrusion system right around the time that it finished construction of the facility it was housed in.

The facility’s integrated control and information has been vital to helping workers optimize quality management and identify production issues.

“Operators can see trending information on the screen to make sure all the equipment and feeders are running right where they should be,” Wilson said. “Any processes that run outside their minimum or maximum setpoints will generate alarms on the operator screen so they can quickly address the issue.”

Both Wilson and Apex team members can access the system to remotely monitor systems and help workers without traveling on-site. This was especially valuable early on as workers were getting the system up and running, and had limited access to local technical support.

“I can look at any of the data points from right here in my office,” Wilson said. “We’ve looked at alarms and helped them diagnose issues, such as when they had trouble getting the proper feed rate or were encountering some initial mechanical issues with the feeder. It’s safe to say remote support helped us reduce some of those early downtime incidents from days into hours.”

Additionally, by using add-on instructions (AOI) in the development of the extrusion system, Apex Control Specialists created plug-and-play functionality for any future changes or additions at the facility. For example, MCPP can add a new feeder to the system in as little as 10 minutes.

Wilson said MCPP may seek to replicate some of the benefits of the modular extrusion system at other facilities.

“The next project we do, we’re going to consider replicating some of the benefits we’ve seen with the modular system,” he said. “It made the project a lot more manageable than a conventional build. I could even foresee using the approach closer to home here in the U.S.”

The results mentioned above are specific to Mitsubishi Chemical Performance Polymers’ use of Rockwell Automation products and services in conjunction with other products. Specific results may vary for other customers.

Allen‑Bradley, CompactLogix, FactoryTalk, PowerFlex and VantagePoint are trademarks of Rockwell Automation Inc.

EtherNet/IP is a trademark of ODVA Inc. Apex Modular Extrusion™ is a trade mark of Apex Engineering, PLLC

Published July 21, 2017

Topics: Chemical
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Loading
Leading Power Company Reduces Threat Response Time
Leading Power Company Reduces Threat Response Time
Case Study
Case Study
Leading Power Company Reduces Threat Response Time
Secured legacy assets—coal, gas, wind, solar, hydro—with Verve by Rockwell Automation platform for real-time risk visibility and faster threat response.
Energy Company Achieved Readiness in Eight Months
Energy Company Achieved Readiness in Eight Months
Case Study
Case Study
Energy Company Achieved Readiness in Eight Months
Energy firm reached CIS Controls maturity in 8 months with unified IT/OT security, compliance, and risk reduction thanks to Rockwell Automation.
Successful Turnkey DCS Migration for Corteva Agriscience
Successful Turnkey DCS Migration for Corteva Agriscience
Case Study
Case Study
Successful Turnkey DCS Migration for Corteva Agriscience
Corteva, a major American agricultural chemical and seed company, migrates its proprietary control system to PlantPAx modern distributed control system.
  1. Chevron LeftChevron Left Rockwell Automation Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Com... Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Case Studies Chevron RightChevron Right
  5. Chevron LeftChevron Left Mitsubishi Chemical Performance Polymers Uses Modular Control System, Manufacturing Intelligence to Launch New Plant in Brazil Chevron RightChevron Right
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
You can update your preferences at any time. For more information please see our Privacy Policy
CloseClose