Visualisation Benefits
Emulate3D users can improve a solution’s time to market, as well as optimise operational productivity through digital machine prototyping.
“It can even be used for virtual commissioning, which has been particularly helpful to navigate site access restrictions during the pandemic, and can save transport costs involved with a whole team travelling to site for commissioning,” said Rockwell Automation account manager, Keegan Houlihan.
Further benefits of using Emulate3D include:
- Space-saving – The software allows engineers to find the optimum plant layout and test multiple options before settling on the best solution.
- Reduced downtime and ‘teething issues’ –By creating an optimal plant layout, and testing all scenarios, there is a reduced chance of experiencing operational issues, or ‘teething issues’ common when new technologies are first installed.
- Energy-saving – By measuring data on all equipment, the software can determine the most efficient way to operate the entire plant, which results in savings on power.
- Safety and standards compliance – The software can help engineers design a solution that is compliant with all relevant safety and industry standards from the outset.
- Reduced risk – being able to accurately test the operations of an entire plant prior to installation means that there is significantly reduced risk of errors or issues after commissioning.
- Maximised throughput and efficiency – automation solutions can be installed in an almost unlimited variety of configurations, so having visualisation software allows engineers to determine which one will create the most throughput, most efficient overall operation, and deliver the best ROI
“Australian manufacturing is growing, and to continue this upward trajectory, manufacturers need to be able to deliver quality, reliability, repeatability, and traceability. Emulate3D is helping us achieve these qualities, and is adding value to our customer offering,” concluded Dunwoodie.