PanelView 5310 graphic terminals provide right-sized HMI solution for machine and equipment builders
MILWAUKEE — Machine and equipment builders are already using tight integration between the HMI and controller to help increase productivity in large applications. With the new Allen-Bradley PanelView 5310 family of graphic terminals, they can now bring these integration benefits to smaller applications.
The PanelView 5310 graphic terminals deliver the same usability benefits and enhanced integration with Logix 5000 controllers as the PanelView 5500 terminals. But the new terminals are specifically designed for applications of up to 50 HMI screens. The terminals are available in 7-inch, 9-inch and 12-inch display sizes. A 6-inch display option will be available in 2018.

Click to download image.
“Engineers can use the PanelView 5310 family to scale a tightly integrated automation system down to smaller applications,” said Mike Moriarty, product manager, Rockwell Automation. “This can help make design, operations and maintenance tasks more efficient. For example, engineers can now reuse controller alarms without creating HMI tags, which can help them reduce configuration time.”
Companies can also use the enhanced integration to create high-speed jog buttons in place of cumbersome hardwired buttons. These auto-diagnosing buttons can interact with the controller at I/O speeds to help reduce downtime and improve productivity.
Other productivity benefits of the PanelView 5310 graphic terminals include the following:
The intuitive Rockwell Software Studio 5000 design environment allows users to create reusable faceplates, screens and custom graphics to help reduce development time. These objects seamlessly integrate with Logix add-on instructions and different user-defined data types.
Emulation capabilities allow engineers to test run projects in the development environment. This can help them make changes without using the PanelView 5000 hardware or disrupting production.
VNC connectivity allows operators to remotely monitor operations via a smartphone, tablet or personal computer. Historical-trending and data-logging features also allow operators to easily troubleshoot issues directly on the panel.
Engineers can load projects onto the PanelView 5310 graphic terminals directly from removable media to more quickly recover information and make project updates without needing to use the Studio 5000 View Designer application.
About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 22,000 people serving customers in more than 80 countries.
Media Contacts
Tiffany Pfremmer
Rockwell Automation
414.382.4814
tbockhop@ra.rockwell.com
Keegan Leddy
Padilla
612.455.1941
keegan.leddy@padillaco.com
Allen-Bradley, Logix 5000, PanelView, Rockwell Software and Studio 5000 View Designer are trademarks of Rockwell Automation Inc.
Published January 11, 2018