Single terminal can reduce need for multiple HMIs or replace PC-based HMI for centralized information-monitoring
MILWAUKEE, Aug. 20, 2015 — Rockwell Automation has released its new Allen-Bradley PanelView Plus 7 Performance graphic terminal to simplify and streamline visualization in large, complex applications. The PanelView Plus 7 Performance terminal expands on the recently released PanelView Plus 7 Standard model with a larger screen option, more processing power, expanded connectivity and greater software support.
“Large machine builders and heavy process industries often require multiple terminals or use PCs to monitor trends and information for their complex applications,” said Scott Oakley, global product manager, Rockwell Automation. “With the PanelView Plus 7 Performance terminal, they can consolidate that hardware into a single interface where hundreds of screens, alarms and tags can be conveniently accessed and monitored.”
New capabilities in the PanelView Plus 7 Performance model include:
Larger screen option: The Performance model has six screen-size options, including a new 19-inch option – the largest to date from Rockwell Automation. The 19-inch screen offers machine builders and end users more display area on which they can design, control and monitor large applications. The Performance model also includes new keypad options to complement the terminal’s standard touch screen.
More processing power: A more powerful CPU supports larger displays and larger applications. While the Standard model supports applications with up to 25 screens and 200 alarms, the Performance model supports applications much larger in size and complexity.
Expanded connectivity: With the addition of an embedded Ethernet switch and two Ethernet ports, the PanelView Plus 7 Performance terminal can support a device level ring (DLR) topology for single-fault resiliency. The terminal also has expanded mobile connectivity. Remote desktop services enable operators and plant managers on the plant floor to connect to centralized enterprise-level systems such as ERP or MES through a thin-client connection. Embedded VNC and FTP servers allow start-up and maintenance technicians to securely access the HMI from a remote location to troubleshoot a problem, walk through setup procedures, review alarming, manage recipes and more. In addition, FactoryTalk ViewPoint software from Rockwell Automation – the embedded webserver technology of PanelView Plus 7 terminals – gives plant operators visibility into plant KPIs using a tablet, smartphone or other mobile device.
Greater software support: With video playback support, machine builders and end users can now incorporate helpful videos into the terminal to support operator training and troubleshooting. Microsoft Office viewers and Internet Explorer support give operators instantaneous access to network-based Office files and HTML pages, such as standard operating procedures, directly from the terminal.
Greater software support:The PanelView Plus 7 Performance terminal also retains the benefits introduced with the PanelView Plus 7 Standard terminal. This includes the ability to save projects and critical machine information on an SD card. For example, machine builders can save a single machine’s configuration on an SD card and re-use it for multiple similar machines, while operators can archive machine data for faster terminal replacements and easier troubleshooting.
Both PanelView Plus 7 models work with FactoryTalk View Machine Edition (ME) software to better handle multiple applications on a single terminal. They also use the same clamping technology that allows easy terminal installation and removal without the use of tools. This reduces installation and maintenance time, and minimizes the risk of overtightening and damaging the terminal during installation.
News Release Assets
Image available upon request or here at box.com.
About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs about 22,500 people serving customers in more than 80 countries.
Media Contacts
Tiffany Pfremmer
Rockwell Automation
414.839.7425
tbockhop@ra.rockwell.com
Leanne Hanson
PadillaCRT
612.455.1776
leanne.hanson@padillacrt.com
Allen-Bradley, FactoryTalk, LISTEN. THINK. SOLVE. and PanelView are trademarks of Rockwell Automation Inc.
Internet Explorer and Microsoft are trademarks of Microsoft Corporation.
Published August 19, 2015