Device Information - Device identity
Displays whether the physical device matches or mismatches with the configuration in the
Overview
view.- Match- The physical device agrees with what is specified in theOverviewview, and all of these must agree:
- Vendor
- Device type(the combination of Product type and Product code for a particular Vendor)
- Major revision
- Mismatch- If the physical device does not agree with what is specified in theOverviewview.
Tip
: Device identity does not take into account the Electronic keying
or Minor revision
settings in the Overview
view. The Generic devices, such as the 1756 devices, always show a Mismatch because the configured Generic Key does not match any target device.Provide Feedback