connections object

Defines the device connections topology of a set of connected devices. The topology models the parent-child relationship among devices.
connections [rootDevice]{ path [bus] { <device> { path [bus] { <device> ... } ... } ... } ... }
Property
Description
rootDevice (required)
Device originating the connections tree.
bus (required)
Defines the route from the originator device to each of the targets.
device
Child device of a parent device connected through the upstream path.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.