Add-On Instructions

Add-On Instructions

Add-On Instructions are best used for encapsulating and reusing complex logic. They allow you to create a self-contained block of logic that can be used multiple times within a program, improving code readability and maintainability.
Add-On Instructions are commonly used for:
Modularizing Code
. Add-On Instructions help break down complex programs into smaller, manageable modules. This makes it easier to troubleshoot and update specific parts of the program without affecting the system.
Improving performance
. By encapsulating logic, Add-On Instructions can reduce the amount of code that needs to be executed during each scan cycle to help improve performance.
Reusability
. Add-On Instructions can be used across different projects to save development time and ensure consistency in logic implementation.
Simplifying maintenance
. Add-On instructions help manage and maintain code to ensure changes in logic only need to be made in one place.
Add-On Instruction can be used by any controller application in a project and enable reuse between different controller applications. Define the instructions, use instructions provided by another user, or copy instructions from another project. Once defined in a project, Add-On Instructions behave like built-in instructions in
FactoryTalk Design Studio
.
Add-On Instructions are commonly used to represent reusable blocks of common code. FactoryTalk Smart Objects are used to represent hierarchical designs of your system.
Add-On Instructions can contain a maximum of 2 megabytes of data.
Add-On Instructions allow you to:
Reuse Code
  • Use Add-On Instructions to promote consistency between projects by reusing commonly used control algorithms.
  • Place the code for an algorithm to be used multiple times in a project or across multiple projects in an Add-On Instruction to make the code modular and easier to reuse.
Provide an understandable interface
  • Place complicated algorithms inside an Add-On Instruction and then provide an interface that is easier to understand by making only essential parameters visible or required.
  • Reduce documentation development time by automatically generating instruction help.
Simplify maintenance
Simplify code maintenance by viewing tag values relative to a specific instance of an Add-On Instruction.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal