FactoryTalk Design Studio Copilot
FactoryTalk Design Studio Copilot is a generative artificial intelligence (Gen AI) assistant designed to answer queries at your request.
Open FactoryTalk Design Studio Copilot from the right-hand side bar.
Use the FactoryTalk Design Studio Copilot to:
- Query the help content, release notes, and error code documentation to answer questions about product features, how to complete tasks, and how to troubleshoot errors and warnings.
- Submit feedback on FactoryTalk Design Studio Copilot responses. UseSend Feedbackat the top right of the response to like or dislike a response and optionally provide details.
FactoryTalk Design Studio Copilot has conversational context and uses the 5 most recent prompts- responses pairs in the chat. When you ask a question, FactoryTalk Design Studio Copilot uses this context to provide the best response. For example, if you ask, “What is a Smart Object”, in one query and then ask, “How do I use them”, in another query, FactoryTalk Design Studio Copilot understands that “them” refers to “Smart Objects”.
The chat history is cleared when you close the project. To clear chat history, select
Clear Chat History
on the top right of FactoryTalk Design Studio Copilot, or select Clear Question and Response
at the top of each response pairing. FactoryTalk Design Studio Copilot may display inaccurate information. Please refer to the FactoryTalk Design Studio Online help to verify its responses.
Provide Feedback