Delete a controller
Delete a controller to remove the controller from the project. The tasks, programs, and allocations to Smart Objects for the controller are removed with the controller. Devices attached to a backplane or bus of the controller are moved to the
Unassigned
folder. Delete a controller from the Devices
explorer.- On the explorer bar, selectDevices.
- InDevicesexplorer, right-click the controller and selectDelete.
- SelectDelete. The controller is removed.
Provide Feedback