Devices explorer

Devices explorer

How do I open Devices explorer?
On the explorer bar, select Devices Icon
Devices
.
Use the
Devices
explorer to view and manage the hardware used in the project. All hardware devices added to the project appear. If no devices are added to the project, the
Devices
explorer is empty.
The
Devices
explorer contains folders:
  • Assigned
    . Controllers in the project.
  • Unassigned
    . Devices in the project that do not have a controller connection. The devices in the
    Unassigned
    folder cannot be used without a controller connection.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.