For (FOR)

For (FOR)

The FOR instruction executes a routine repeatedly.
When enabled, the FOR instruction repeatedly executes the Routine until the Index value exceeds the Terminal value. This instruction does not pass parameters to the routine.
The step value can be positive or negative. If it is negative, the loop ends when the index is less than the terminal value. If it is positive, the loop ends when the index is greater than the terminal value.
Each time the FOR instruction executes the routine, it adds the Step size to the Index.
Be careful not to loop too many times in a single scan. An excessive number of repetitions can cause the controller’s watchdog to timeout, which causes a major fault.
Available Languages
Ladder Diagram
Ladder Diagram_For (FOR)_v1
Operands
Ladder Diagram
Operand
Type
Format
Description
Routine name
ROUTINE
tag
Subroutine that is invoked each time the FOR loop executes.
Index
DINT
tag
Counts how many times the routine has been executed
Initial value
SINT
INT
DINT
immediate
tag
Value at which to start the index
Terminal value
SINT
INT
DINT
immediate
tag
Value at which to stop executing the routine
Step size
SINT
INT
DINT
immediate
tag
Amount to add to the index each time the FOR instruction executes the routine
Affects Math Status Flags
No
Major/Minor Faults
A major fault will occur if:
Fault type
Fault code
The nesting level limit > 25
4
94
the subroutine is an SFC and it is already executing (recursive call)
4
82
See Common Attributes for operand-related faults.
Execution
Condition/State
Action
Prescan
The instruction will prescan the named subroutine if it has never been prescanned before.
Tip:
If recursive FOR instruction exist to the same subroutine, or multiple FOR instruction exist (non-recursive) to the same subroutine, the subroutine is pre-scanned only once. This is also true if the subordinate was prescanned by a JSR.
Rung-condition-in is false
N/A
Rung-condition-in is true
See the following FOR Flow Chart (True).
Postscan
The instruction will postscan the named subroutine exactly once.
FOR Flow Chart (True)
FOR Flow Chart True
Examples
When enabled, the FOR instruction repeatedly executes routine_2 and increments value_2 by 1 each time. When value_2 is > 50000 or a BRK instruction is enabled, the FOR instruction no longer executes routine_2.
FTStudio-FOR-LD-EX2
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal