Special Instructions

Special Instructions

The special instructions perform application-specific operations.
Available Instructions
If you want to:
Use this instruction:
Compare data against a known, good reference and record any mismatches.
Compare data against a known, good reference, record any mismatches, and update the reference to match the source.
Pass the source data through a mask and compare the result to reference data. Then write the source into the reference for the next comparison.
Control a PID loop.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal