Allocate Entitlements

Once purchased, entitlements
must
be allocated to the specific application or service for which they were purchased.
To Allocate an Entitlement
  1. From the FactoryTalk Hub menu in the upper left of the screen, select
    View Entitlements
    . The View Entitlements page appears.
  2. In the FactoryTalk Hub page title bar, select and select
    View Entitlements
    . The new entitlement appears at the top of
    All Entitlements
    under
    Available for Allocation
    .
  3. Verify that the correct organization name appears on the right side of the FactoryTalk Hub title bar.
  4. Locate the entitlement that you want to assign to your organization and select
    Allocate
    next to the entitlement row.
  5. Ensure that the entitlement, organization and allocated entitlements quantity are correct, then select
    Review Allocation
    .
  6. Confirm the allocation when prompted. The entitlement is allocated to the organization.
  7. In the upper left corner of the FactoryTalk Hub web page, select
    Home
    .
  8. The allocated entitlement is now available in the application to which it was allocated. Additional steps may be required for your application. See the application's documentation for details.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.