Configure a localization dictionary
Support a multilingual user interface by configuring the appropriate localization dictionaries.
- InProject view, expandTranslations.
- Double-clickLocalizationDictionary1.
- Add the it-IT locale.For more information, see Add a locale language to a localization dictionary.
- Translate strings.For more information, see Translate a string.
![](/content/dam/dita/en/factorytalk-optix/1-00/_images/ColorCodeAlarmTranslation2.png/_jcr_content/renditions/original)
![](/content/dam/dita/en/factorytalk-optix/1-00/_images/ColorCodedAlarmTranslation.png)
Provide Feedback