Create a severity color converter
Create a converter that translates alarms severity into colors.
- Create the converter:
- InProject view, right-clickConvertersand select .
- Hover-over the converter, select, and enterEditSeverityColorConverter.
- Configure the converter:
- Double-clickSeverityColorConverter.
- In the central pane, next toValues, selectStringand selectColor.TIP: If you do not see the required option, select theShow allcheck box.
- Add another row by selecting.Add
- Enter the following values:Keys (UInt32)Values (Color)1#ff00000#0664c2
![](/content/dam/dita/en/factorytalk-optix/1-00/_images/ColorCodedAlarmsDashboardConverter.png/_jcr_content/renditions/original)
Provide Feedback