Create a motor values widget (type)
Create container elements for gauges, labels, and text boxes related with selected motor values.
- Crate the motor values widget panel:
- InProject view, right-clickUIand select .
- Hover-over the panel, select, and enterEditMotorValuesWidget.
- Create an alias to the motor instances:
- InProperties, at the top, selectand selectAddAlias.
- Double-clickAlias1and enterMotor.
- Create a dynamic link betweenKindandFor more information about dynamic links, see Create dynamic links.
- Crate a motor speed panel:
- InProject view, right-clickMotorValuesPanelWidgetand select .
- Hover-over the panel, select, and enterEditMotorSpeedPanel.
- Crate a motor acceleration panel:
- InProject view, right-clickMotorValuesWidgetand select .
- Hover-over the panel, select, and enterEditMotorAccelerationPanel.
Provide Feedback