Develop a gauge with a localized engineering unit
Create a linear gauge that displays the current temperature in a format adjusted to the logged in user.
Application example - Celsius degrees (it-IT)
![](/content/dam/dita/en/factorytalk-optix/1-00/_images/LocalizedEngineeringLabel2.png/_jcr_content/renditions/original)
Application example - Fahrenheit degrees (en-US)
![](/content/dam/dita/en/factorytalk-optix/1-00/_images/LocalizedEngineeringLabel.png/_jcr_content/renditions/original)
NOTE:
Download a sample project:
LocalizedEngineeringUnitGauge.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example
![](/content/dam/dita/en/factorytalk-optix/1-00/_images/LocalizedEngineeringUnitGaugeDesign.png/_jcr_content/renditions/original)
In
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
FactoryTalk Optix Studio
, select ![Run](/content/dam/dita/en/factorytalk-optix/1-00/_images/toolbar_run_icon.png/_jcr_content/renditions/original)
Run
Provide Feedback