Create a clock label
Create a label that displays the current time.
- Create the label:
- InProject view, right-clickMainWindow (type)and select .
- Hover-over the label, select, and enterEditClockLabel.
- Configure the label
- IMPORTANT:While performing this step, in the dynamic link dialog, at the bottom, from theFormatdrop-down menu, select a time format.For example, selecth:mm:ss [AM/PM].InProperties, create a dynamic link betweenTextand .For more information about dynamic links, see Create dynamic links.
- InProperties, create a dynamic link betweenVisibleand .For more information about dynamic links, see Create dynamic links.
Provide Feedback