Project view
Project view
displays the contents of the FactoryTalk Optix Application
in a tree structure.Project view
contains buttons for navigating the contents of the application. Some buttons appear in the title bar of Project view
. Other buttons appear in the selected object.Item | Description |
---|---|
![]() | Navigate backward . Go to the previously selected pane. |
![]() | Navigate forward . Go to the next selected pane. |
![]() | Split project view . Divide Project view into two panes. |
![]() | Add new . Create a node inside the selected node. |
![]() | Delete . Remove the selected node and the nodes that it contains. |
![]() | Lock the selected child node to hide it from Project view . You cannot edit locked child nodes. |
![]() | Unlock the selected child nodes to display it in Project view . You can edit unlocked child nodes. |
![]() | Open the selected object in the dedicated editor. Only certain object types have a dedicated editor. |
Provide Feedback