Display information model graphs
Visualize information models of
FactoryTalk Optix Studio
projects in the form of graphs.
TIP:
For more information about project information models, see Information model.
Prerequisites
- Install an application that displays graphsDGMLgraphs, such as Microsoft Visual Studio with the DGML Editor component.TIP: For more information aboutDGMLfiles, see Directed Graph Markup Language (DGML) reference - Visual Studio (Windows) | Microsoft Learn.
- To display information model graphs
- InProject view, right-click the project node.
- SelectModel analysisand then select either:
- Information model graph (Project only). Visualize only nodes, types, and references related to the user project.
- Information model graph (Ignore OPCUA/Core namespaces). Visualize nodes, types, and references of the user project andFTOptixmodules namespaces, except OPC-UA and Core namespace.
- Information model graph. Visualize all nodes, types, and references of any namespace.
Information model graph example
![](/content/dam/dita/en/factorytalk-optix/1-00/_images/info_model_graph.png/_jcr_content/renditions/original)
Provide Feedback