Animation properties

Animation properties

Configure animations by editing animation properties.

Number animation

A simple animation based on a variable value change over specific time.
Property
Description
From
Start value of the range.
To
End value of the range.
Duration
Duration of the animation in milliseconds.
Interpolation
The type of interpolation when animation value changes.
Target
Target node of the animation.
Running
Boolean value.
Loops
Number of consecutive animation playbacks. The
-1
value sets continuous animation playback.

Sequential animation

Groups of animation executed in a sequential order.
Property
Description
Running
Boolean value.
Loops
Number of consecutive animation playbacks. The
-1
value sets continuous animation playback.

Parallel animation

Groups of animation executed in a parallel order.
Property
Description
Running
Boolean value.
Loops
Number of consecutive animation playbacks. The
-1
value sets continuous animation playback.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.