Known anomalies in this release

The list identifies the known anomalies in
FactoryTalk Optix
version 1.4.1.
Use the identification information in parenthesis to track the anomaly in future releases or for reference when receiving assistance from Customer Support with a related issue.
Compute Module with multiple backplanes in controller path unable to communicate with controller
The Compute Module cannot communicate with the controller if there is more than one Backplane in the controller path. For example, the module is unable to communicate with the controller if the path is Backplane\1\A\10.220.173.66\Backplane\3. However, paths resembling either Backplane\3 or Backplane\1\A\10.220.173.66 allow the module to communicate with the controller.
This anomaly first identified in version 1.2.0.
Image does not appear at runtime [3140280]
If an image file in a project does not appear in the runtime application, use a third party application to resize the image and make it smaller.
This anomaly first identified in version 1.3.0.
No error appears when misconfiguring a string as a Discrete Input for a Modbus Station and all other tag reads fail [2351429]
Assigning a string tag to a Discrete input memory area does not display an error message and causes read errors on all tags for the Modbus Station containing the misconfigured tag.
This anomaly first identified in version 1.3.0.
Renaming a user-defined library using OneDrive may result in synchronization errors [2348900]
OneDrive is not recommended for storing user-defined libraries and may result in synchronization errors and duplicate files when renaming libraries. If attempting to use OneDrive to rename a library, unlink OneDrive when renaming the library. To unlink OneDrive, see Turn off, disable, or uninstall OneDrive.
This anomaly first identified in version 1.3.0.
Custom library elements do not appear without restarting FactoryTalk Optix [2371413]
Elements added to a custom library do not appear in
Libraries
search until you restart FactoryTalk Optix.
This anomaly first identified in version 1.3.0.
Some videos may not play on computers running Microsoft Windows [2212837]
If you emulate a project on a computer that is running
Microsoft®
Windows®
, some videos may not play. Videos will play if you deploy the project to a device.
This anomaly first identified in version 1.1.0.
Unable to connect to certain Logix Controllers over ControlNet [3385425]
When trying to connect to one of the following controller types over a ControlNet network:
  • 1769-L35CR
    CompactLogix
  • 1768
    CompactLogix
  • 1768
    Compact GuardLogix®
You cannot route through a 1756-ENxT(R) module to connect to the controller. You need to use one of the following EtherNet/IP modules:
  • 1756-ENBT
  • 1756-EWEB
Min and Max values do not display for Date Time and Duration types [3370306]
FactoryTalk Optix
does not support Min and Max values for Date Time and Duration types. Do not import Min or Max values for these types.
This anomaly first identified in version 1.4.0
Unable to create a project in a network folder
Attempting to create a project in a network folder displays an error indicating that
FactoryTalk Optix
cannot rename the project template.
This anomaly first identified in version 1.4.0.
Runtime tool cannot deploy to second computer if the computer name contains special characters [3303008]
Do not use Chinese or European special characters in computer names.
This anomaly first identified in version 1.4.0.
Unable to compile NetSolution [3327229]
NetSolution does not compile without internet access. Establish an internet connection to retrieve the required components.
This anomaly first identified in version 1.3.0.
Emulator unable to connect the InfluxDB server via VPN [3350681]
Use Runtime Tools to connect the InfluxDB server via VPN. You can then deploy the project to the selected device.
This anomaly first identified in version 1.4.0.
Unable to debug DesignTime NetLogic from Visual Studio Code [3511011]
The C# extension for Visual Studio Code was updated and some issues were detected with the recent versions. To debug design time NetLogic from Visual Studio Code, revert the C# extension to version 2.4.4 or earlier.
This anomaly first identified in version 1.3.1.
Rotated accordions may not appear as intended [1891903]
Rotated accordions are not supported.
This anomaly first identified in version 1.4.0.
Broken references when importing widgets from the template library [3634901]
NetLogic defined on a child of a widget will not be imported from the template library when it contains the same name as other NetLogic used within the project resulting in broken NetLogic references.
This anomaly first identified in version 1.4.0.
Application does not automatically start after project upload when Running as a Service [3628522]
An application that terminates after uploading the project with application files to FactoryTalk Optix Studio will not automatically restart when running FactoryTalk Optix as a Service. Manually start the runtime serve or redeploy the application.
This anomaly first identified in version 1.4.0.
Cannot deploy an application when NetLogic script is open [3545605]
Application deployment will abort with error message “Unable to prepare project source archive: copy” if any NetLogic script is open. Close the script and deploy the application again.
This anomaly first identified in version 1.4.0.
Cannot communicate with a controller using the WAN port on an OptixPanel or Embedded Edge Compute module [3213290]
The OptixPanel and Embedded Edge Compute module cannot communicate with a controller using the WAN port. The OptixPanel uses port 2 for WAN and port 1 for LAN and the Embedded Edge Compute module uses port 1 for WAN and port 2 for LAN. Use the LAN port to communicate with the controller.
This anomaly first identified in version 1.4.0.
An advanced SVG image with opacity defined at the group level is not shown correctly [3249226]
Opacity applied to sub-elements of an advanced SVG image is not shown as expected when running in the emulator or OptixPanel when it is defined at the group level. Apply the opacity at the element level for expected results.
This anomaly first identified in version 1.4.0.
Engineering unit converter does not show converted values [3558734]
Engineering unit converters set directly on a property with the raw max and min values left at the default 0 do not show converted values. Create a custom engineering unit converter under the converters folder and reference it when creating an advanced dynamic link instead.
This anomaly first identified in version 1.4.0.
Project retentivity does not work as expected using multiple projects with the same name [3540833]
Project retentivity does not work as expected using multiple projects with the same name in different locations. Ensure projects have unique names when using retentivity.
This anomaly first identified in version 1.4.0.
IDE display issues when switching between local and RDP sessions [2294982]
A blank screen may appear in the Desktop IDE when toggling between local and remote desktop sessions.
This anomaly first identified in version 1.4.0.
Trend range update may affect result table [3612644]
Updating the
Ranges
tab in the Advanced Trend widget may affect the result table.
This anomaly first identified in version 1.4.0.
Non-variable event field causes runtime error [3612644] 
A discrepancy in event argument handling causes the return of non-variable nodes and displays the error "The event field resolves into a non-variable”.
This anomaly first identified in version 1.4.0.
Image may not refresh on web presentation engine [3478736]
The ImageRefresher script does not work as expected using the web presentation engine.  To display the image correctly, the web browser needs to be refreshed manually.
This anomaly first identified in version 1.4.0
Special characters not always supported [2123530]
Special characters are supported in PDF filenames and FTP Server usernames but are not supported in Git repository names, ODBC database names, or when using the Microsoft Pinyin input method on the device or at design time in FactoryTalk Optix Studio web editor.
This anomaly first identified in version 1.2.0.
New or deleted tags that are changed online in a controller running V20 firmware not detected by FactoryTalk Optix [3671499]
If you use the RA EtherNet/IP Driver with a controller running V20 firmware, FactoryTalk Optix will not detect new or deleted tags when those changes are done while online with the controller.
To resolve this, deploy your project again and in
Project already exists
, select
Replace
.
IMPORTANT: Replacing a project replaces all application files.
This anomaly first identified in version 1.4.0.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.