Add a subdevice

  1. In the
    FactoryTalk Remote Access Manager
    , access the
    Explorer
    Domain view
    section.
  2. In the domain left pane, select the primary device on which the subdevice is dependant.
  3. Next to the primary device, in its same line, select . Alternatively, select the three dots at the top of the screen and select
    Add subdevice
    .
  4. A
    Create Subdevice
    dialog window opens. Enter the subdevice
    Name
    and
    IP Address
    .
    NOTE: The subdevice IP address must be compatible with a subnet that is reachable by the remote device.
  5. Select
    Save
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.