Invite users to an organization
An organization provides a space for users to interact with resources.
Once an organization has been created, users can be invited to your organization:
NOTE:
See Organizations, domains and domain subfolders for further information on this subject.
- In FactorytalkHub.com, select the
menu at the top left corner, then select
Invite users. You will be redirected to theInvite userspage. - Expand theResourcepull down menu and selectService: FactoryTalk Remote Access.
- Expand theRoledropdown menu and select theAdminrole.
- In the text box, type the email addresses of the people in your organization who will be administrators in FactoryTalk Remote Access domains.NOTE: Use a semicolon to separate entries in a list of email addresses.
- Expand theRoledropdown menu and selectContributor.
- In the text box, type the email addresses of the people in your organization who will be contributors in FactoryTalk Remote Access domains.
- SelectSend Inviteto send an email invite to the specified user accounts.
Accept invitation
The owner of an organization may send invitations via email to ask a user to join an existing organization. The recipient's email address must be associated with a MyRockwell user account.
NOTE:
If you do not have a MyRockwell Account, you can set it up before attempting to join the organization or during the join process. See Create an organization and a domain for further information on this subject.
The invitation email includes:
- The name of the domain owner who invited you to the organization.
- The name of the organization you are joining.
To accept the invitation:
- Click theJoin nowbutton in the email to connect to FactoryTalk Hub and sign in.
- AnInvitation Accepted Successfullymessage displays.
- SelectOK.
Provide Feedback