Routing rules
Routing rules consist of a set of criteria determining the path that data packets take from the source to destination across one or more networks. Routing rules are a fundamental aspect of networking, playing a crucial role in determining how data is transmitted between devices on a network.
Once a remote VPN connection is established, the devices connected to LAN 1 become immediately reachable. Instead, the devices connected to LAN 2 are accessible only upon routing rule configuration through
FactoryTalk Remote Access Manager
.Configuration
To create, modify and cancel static routing rules through
FactoryTalk Remote Access Manager
, access and select a device on the left pane. Then, select Routing rules
on the right pane and click on the circled plus
button.The
Create routing rule
window shows up. It includes three fields:- Subnet IP: The subnet that you wish to reach.
- Subnet Mask: The mask of the subnet that you wish to reach.
- Gateway IP: The gateway to which any requests to access a specific subnet are forwarded (for example, 192.168.11.113).
You can associate a number of routing rules to a device. They are shown in the
Routing rules
pane.In the example shown, one static routing rules has been applied.
NOTE:
When a VPN connection is no longer active, the added routing rules are automatically deleted.
Example
To allow the computer providing remote assistance to reach a device on LAN 2 configure a routing rule as per below:
- Subnet IP: 10.65.0.0
- Subnet Mask: 255.255.0.0
- Gateway IP: 192.168.11.113
Provide Feedback