Router
This hardware component allows for remote access or assistance on industrial devices where machinery plants are lacking any wired connection by means of 4G modems and WiFi.
The router integrates greatly into any automation system without impacting the setup of the devices included therein, since no configuration adjustment is required for them.
Once installed, you can configure and manage the router connection or create and manage any subnets through a router System Manager and
FactoryTalk Remote Access Manager
. In fact, routers allow to set up NAT and routing rules outside VPN.Provide Feedback