MOTION_INSTRUCTION Data Type

MOTION_INSTRUCTION Data Type

You must define a motion control tag for each motion instruction that you use. The tag uses the MOTION_INSTRUCTION data type and stores status information about the instruction.
Mnemonic
Data Type
Description
FLAGS
DINT
Use this DINT to access all the status bits for the instruction in one 32-bit value.
For this status bit
Use this bit number
EN
31
DN
29
ER
28
PC
27
IP
26
AC
23
DECEL
1
ACCEL
0
EN
BOOL
The enable bit indicates that the instruction is enabled (the rung-in and rung-out condition is true).
DN
BOOL
The done bit indicates that all calculations and messaging (if any) are complete.
ER
BOOL
The error bit indicates when the instruction is used illegally.
PC
BOOL
The process complete bit indicates that the operation is complete.
The .DN bit sets after an instruction has completed execution. The .PC bit sets when the initiated process has completed.
IP
BOOL
The in process bit indicates that a process is being executed.
AC
BOOL
The Active Bit lets you know which instruction is controlling the motion when you have instructions queued. It sets when the instruction becomes active. It is reset when the Process Complete bit is set or when the instruction is stopped.
ACCEL
BOOL
The .ACCEL bit indicates that the velocity has increased for the individual instruction that it is tied to, that is, jog, move, gearing.
TrackingMaster
BOOL
Indicates that the Slave Coordinate System is tracking the Master Axis (only used in Master Driven Mode).
CalculatedDataAvailable
BOOL
Indicates that the requested data has been returned in the Calculated Data array element and that the
Logix Designer
application has updated the output data in the Calculated Data parameter. Only one status bit is used to indicate all Calculated Data is available.
DECEL
BOOL
The .DECEL bit indicates that the velocity has decreased for the individual instruction that it is tied to, that is, jog, move, gearing.
ERR
INT
The error value contains the error code associated with a motion function.
See Error Codes (ERR) for Motion Instructions.
STATUS
SINT
The status of any message associated with the motion function.
Message Status
Description
0x0
The message was successful.
0x1
The module is processing another message.
0x2
The module is waiting for a response to a previous message.
0x3
The response to a message failed.
0x4
The module is not ready for messaging.
STATE
SINT
The execution status value keeps track of the execution state of a function. Many motion functions have several steps and this value tracks these steps. The execution status is always set to 0 when the controller sets the EN bit for a motion instruction. Other execution states depend on the motion instruction.
SEGMENT
DINT
A segment is the distance from one point up to but, not including the next point. A SEGMENT gives the relative position by segment number as the Cam is executing.
EXERR
SINT
Extended error code - use it for more information about an error.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal